Hi,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Hi Srkar,
I had purchased a similar PLC kit from TI and tried working with it. I faced similar probles as yours. The purpose of my testing was to determine the speed at which data transfer occur between the 2 modems. Hence I tried the file transfre mode, but the error keeps on corrupting the received file.
Can anybody please help?
Best regards
Mike.
I've sent this to the PLC team, unfortunately much of the US team is on vacation this week.
PLC team has requested that if you have any issues please send an email directly to
The test sequence is fine.
However, since its on power line, it is best to select MCS with FEC on. For example, select DBPSK+FEC. This should solve the problem of errors in file transfer
To test the throughput, file transfer is not a good measure since this involves the delay in the PC application. The best is to use PHY test mode and monitor statistics panel for throughput number.