Part Number: TMS320F28377D
Hi expert,
My customer is using F28377DPTPT on their current product. They doing ADC sample on both CPU1 and CPU2 (12bits single ended). On CPU1, they sampling at 16kHz and 32kHz with multiple trigger source. On CPU2, they sampling around 16kHz (shift around this point) with single trigger source.
They are not being able to do synchronous sampling like mentioned in TRM. So my questions are:
Q1: If there are any method to do synchronous sampling in this case?
Q2: What is the worst case would be on ADC performance in this case?
Q3: Will the picture below show the worst case?
Thanks