This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335: TMS320F28335 SPI pull up question

Part Number: TMS320F28335


TMS320F28335 : 

Do I need to have external pull up on the SPI pins of the TMS320F28335 device?

The TMS320F28335 device have the internal pull up on those pins but not sure the external one are needed?

Thanks.

  • Hello Hai,

    External pull ups are not necessary. The internal pull up is sufficient for most cases. That being said, if you have a noisy application, having the external pull up would be additional guard against noise propagating into the transmission.

    Thanks,
    Mark