Part Number: TMS320F28030
Hi I'm new to the C2000,
I need to create a PWM waveform with a duty cycle of < 50 percent at a freq of 35khz
Using a PWM is not an option, which forces the use of a timer with a interrupt.
Is it possible to load timer counter with two different time periods (high/low) in the interrupt.
the sample code provided does not address the above, do you have something else available?
thanks