Hi ,
We are working on power factor correction using TMS320f28069. We have custom hardware and control card. We are facing following problems.
1. When are turning on AC mains power to Power board of PFC then JTAG is disconnecting.
2. The main problem when controller is trying to do PFC that is following the current the voltage the clock frequency of CPU is getting changed from 80MHz to 4Mhz and then it is tripping.
what are the cause of this type of problems ?? and any possible solution.?