Part Number: TMS320F28379D
Other Parts Discussed in Thread: OPA320, OPA350
Hello Team C2000,
I have a question WRT external REF (like for VREFHIA) circuitry spec'd in the datasheets and the TRMs for these devices..
The datasheet (http://www.ti.com/lit/ds/symlink/tms320f28379d.pdf ) Table 4-1 says for pins like (VREFHIA).. "ADC-A high reference. This voltage must be driven into the pin from external circuitry. Place at least a 1-µF capacitor on this pin for the 12-bit mode, or at least a 22- µF capacitor for the 16-bit mode. This capacitor should be placed as close to the device as possible between the VREFHIA and VREFLOA pins. NOTE: Do not load this pin externally." w/ no mention of a series resistor to be included.
The TRM (http://www.ti.com/lit/ug/spruhm8g/spruhm8g.pdf ) section 10.3.4 says the following.. "A capacitor between the high and low reference pins should be placed on the PCB as close to the pins as practical to help absorb high frequency currents. A series resistor (typically <1Ω ) in series with this capacitor may be necessary to ensure op-amp". Two issues w/ this..
1. The TRM recommends a 1Ohm resistor in series w/ the cap on the REF pins while the datasheet does not.
2. The referenced quote in the TRM is an incomplete sentence.. there is nothing after "to ensure op-amp"... what is the rest of the sentence?
What is the overall recommend.. a 1Ohm resistor or not?
Thanks, Merril