Part Number: TMS320F28035
Hi after IER=0x20 is added to main, the source does not enter the timer0 interrupt.
After removal, the timer interrupt is working. Why does IER=0x20 effect timer0 interrupt and what is it's purpose?
the code s from the SPI loopback Int
PieCtrlRegs.PIECTRL.bit.ENPIE = 1; // Enable the PIE block
PieCtrlRegs.PIEIER6.bit.INTx1=1; // Enable PIE Group 6, INT 1
PieCtrlRegs.PIEIER6.bit.INTx2=1; // Enable PIE Group 6, INT 2
IER=0x20;