Part Number: TMS320F28027
Tool/software: Code Composer Studio
Hello,
I have a signal with 3 different levels i want to measure the time period for each level. I have a question is it possible to calculate the time using eCAP? Because for eCAP to consider an edge in signal the voltage difference should be more than 1 V (I have worked out with this). if I have a signal with 0 V, 1.5 V and 3 V. Is it possible to determine the interval length for each voltage level? I have the signal shown in attached figure.
I am using the signal like this now. But some of the values of capture register are negative.
Regards,
Mohsin Ejaz Ahmad