This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSACDCKIT

Team, a few questions on the kit:

- the EVM uses the F2808 processor (not the F28035 I am going to be using). Would it be possible to swap the control card for one that has the Piccolo processor in it?
- can the code be ported to the 28035 processor without modifications (or if they are modifications, what are they)
- the 28035 is a 60 MHz processor and the 2808 is a 100 MHz processor. Would the code be able to run on the slower processor or would I have to decrease my sampling time accordingly?

Thanks

Viktorija

  • Viktorija Cecil said:
    - can the code be ported to the 28035 processor without modifications (or if they are modifications, what are they)
    - the 28035 is a 60 MHz processor and the 2808 is a 100 MHz processor. Would the code be able to run on the slower processor or would I have to decrease my sampling time accordingly?

    Viktorija,

    I suggest the customer read through the TMS320F280x to TMS320F2802x/TMS320F2803x Migration app note: www.ti.com/lit/SPRAB40

    The ADC differences are highlighted in section 9.2.  There are quite a few changes/improvements made to the ADC module on 2803x over 280x devices.

    Regards,

    -Lori

  • Viktorija Cecil said:
    - the EVM uses the F2808 processor (not the F28035 I am going to be using). Would it be possible to swap the control card for one that has the Piccolo processor in it?

    Vikotrija,

    I'm looking into this - will let you know as soon as I find out.

    -Lori