Other Parts Discussed in Thread: TMS320F28335
I am trying to program the TMS320F28335 using serial port. To the best of my knowledge I have to set the XA15, XA14 and XA13 to HI and XA12 to LOW at the power up.
There are two pins available for SCITXDA (pin 2 and pin 148) and two pins for SCIRXDA (pin 141 and pin 145). Are these pins selectable? or we have to program via certain pins only. How the hardware knows which pins are used for SCITXDA and SCIRXDA?
Thanks
Tom E