This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using the USB Port of "Piccolo controlSTICK USB evaluation tool" for User Application

The USB port of the  "Piccolo controlSTICK USB evaluation tool" is used for code development and debugging during the code development.

Is it possible to use the USB port to communicate with the user GUI when the coding is done and the code is downloaded into the flash memory?