Part Number: TMS320F280049C
Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
Hi everyone,
I’d like to request a support on a example project that I’m trying to run on F280049 controlCARD unsuccessfully.
I’m trying to run the serial flash utility provided in the “C2000Ware_1_00_06_00_Software” software pack:
C:\ti\C2000Ware_1_00_06_00_Software\utilities\flash_programmers\serial_flash_programmer
My hardware is composed by the F280049 controlCARD inserted in the 120HSEC connector of the experiment kit board (both boards are powered with two PC-USB ports).
I set the F280049 microcontroller in “Boot from SCI” mode with the following GPIOs configuration:
I connect the mini-usb connector to my PC (GIPO-28 SCI-RX, GPIO-29 SCI-TX). The COM is recognized as COM1 port.
I launch the command from “commands prompt console” using the following files as parameters:
- C:\ti\C2000Ware_1_00_06_00_Software\utilities\flash_programmers\serial_flash_programmer\f28004x_fw_upgrade_example\flashapi_ex2_sci_kernel.txt
- C:\ti\C2000Ware_1_00_06_00_Software\utilities\flash_programmers\serial_flash_programmer\f28004x_fw_upgrade_example\led_ex1_blinky.txt
The download always freezes at the same point (If I reset the device and I try again to launch the download, I obtain always the same issue).
What am i doing wrong?
Thank you very much for your support.
Fabrizio