I have an TMDSPLCKITV4-CEN.
I am performing some file transfers using the Intermediate GUI between two PLC modems.
When the file transfer is complete, i draw the values of SNR, RSSI and LQI from the log file and the error .
Sometimes those data are repeated, having several values and sometimes all those values are different.
Which value should i take? where can i find any information about the interpretation of the data in the log file?