Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
Hi,
I am trying to connect C2000 launchpad XL TMS320F28379D to elmo driver.
So I started step by step
I wanted to check how does CAN work
So I pulled up the external CAN example and as mentioned in the example
GPIO 30 (CAN A RX) was connected to directly to GPIO 8 (CAN B TX) using jumper
GPIO 31 (CAN A TX) was connected to directly to GPIO 10 (CAN B RX) using jumper
Is this approach correct?
Do I have to change frequency or anything else
Also the pin numbers I have used is as below, I have pulled them from schematic
GPIO 30 - pin 46
GPIO 31 - pin 45
GPIO 10 - pin 76
GPIO 8 - pin 78