Part Number: LAUNCHXL-F28377S
Other Parts Discussed in Thread: CONTROLSUITE, BOOSTXL-BUCKCONV, POWERSUITE
Tool/software: Code Composer Studio
Hi,
I followed the instructions to get the BOOSTXL-BUCKCONV booster pack up and running together with F28377S launchpad. I am able to import the project into CCS (using CCSv8.2.0) from controlSUITE - either directly from controlSUITE, or from TI Resource Explorer Classic or via project import, but in all cases whenever I open main.cfg with xgconf I do not see the GUI, only empty white space.
I have seen a thread on e2e with similar issue, but in my case I do not have a jxbrowser task and I am also not able to copy and check the link of PowerSuite, because in my case if I right click PowerSuite in main.cfg (after enabling grace developer features) I only get "about:blank", so basically there is no URL copied, which I could check/follow in chrome for example.
Please let me know, how I can enable the GUI view of Solution Adapter from powerSUITE within CCS main.cfg xgconf view?
- CCSv8.2.0
- controlSUITE v3.4.9
Many thanks and best regards,
Gregor