This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TMS320F28379D: Nanosecond (ish) Sub-microsecond Delay Macro

Part Number: TMS320F28379D

Tool/software: TI C/C++ Compiler

I looked for and couldn't find an example of a sub microsecond delay macro or function.  Though I did see a few related questions.

The method isn't perfect.   Hopefully this will be useful for anyone else in need of reliable delays less than 1 microsecond.

Spacing in several areas of the final macro are important.

#define HASH #
#define GLUE(x) x
#define QUOTES_HELPER(x) #x
#define QUOTES(x) QUOTES_HELPER(x)

// On the TMS320F28379D there are 15 ns of overhead, and each nsChunk is 5 ns (200 MHz).
// e.g. nsDelay(0,D1) will delay for 15 ns, the overhead amount.
// nsDelay(1,D2) for 20 ns, nsDelay(2,D2) for 25 ns, and so on.
// The 'label' parameter must be unique for each instance of nsDelay()

#define nsDelay(nsChunk, label) asm(QUOTES(label: RPT GLUE(HASH)GLUE(nsChunk) || nop))