Part Number: TMS320F28377S
Other Parts Discussed in Thread: TMS320F28075
Hi
I'm testing USB boot with 28377s
I saw ' TMS320F28075: USB Boot Mode ' thread...
and I do exactly same as what Stanly Admas did..
USB Boot & Flash Firmware .. everything works well..
and I apply below code to my Custom RTOS.
just run 'Usb_Boot code' in a task
-------------------------------------------
USB_Boot(0x0C5A);
asm(" LB 0x00");
--------------------------------------------
and I saw below message..
----------------------------------------------------------
Manufacturer: Texas Instruments
Product ID: TMS320F28x7x USB Boot Loader
Serial number: 2
Sending 14206 bytes of data from file f2837xD_fw_upgrade_example\F2837xD_usb_fla
sh_kernels_cpu01_origin.dat... done!
14206 out of 14206 bytes sent
Success!
Manufacturer: Texas Instruments
Product ID: TMS320F28x7x USB Boot Loader
Serial number: 2
Sending 190134 bytes of data from file Application.dat...
Error sending bulk transfer: 0x001f
0 out of 190134 bytes sent
USB operation failed!
-------------------------------------------------------------
any suggestion??
What does Error code(0x001f) mean ?
thanks in advance..
Moonsun