Part Number: TMS320F28075
Hi expert,
My customer testing their digital power product with NMI watchdog reset happens on one of their several prototype machine.
In the failing machine, let's call it "model F", when it operating at a relative low power level - no problem happens. But once they add up to load to a high level, in second, a reset happens. They changed F28075 chip on their device once but the problem persists.
We checked the NMISHDFLG register in this case and find FLUNCERR bit is set which indicate some “FLASH uncorrectable errors” happens on the device.
They program their device using our debugger and they do store some channel parameter in flash sector to do calibration.
I am now asking them to check below registers to further inspect this issue: UNC_ERR_ADDR_LOW, UNC_ERR_ADDR_HIGH, ERR_STATUS, ERR_INTFLG
Do you have any suggestion on this? For this project is already in final stage before MP. Please help me with any suggestions you have!
Sheldon
Thanks!