This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379S: question about HWBIST

Part Number: TMS320F28379S

Hi Champ,

From  the F2837xS TRM  , there have below description, could you advise the detail about the special boot ROM flow and HWBIST flow?

Thanks!

2.3.9 Hardware BIST Reset (HWBISTRS)
The Hardware Built-In Self-Test (HWBIST) module tests the functionality of the CPU. At the end of the
test, it resets the CPU to return it to a working state. This reset (HWBISTRS) only affects the CPU itself.
The peripherals and system control remain as previously configured. The CPU state is restored in
software as part of a special boot ROM flow. For more information on the HWBIST flow, contact your local
TI representative.