This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8301-69M-KIT: DRV8301-69M-KIT Motor Capability

Part Number: DRV8301-69M-KIT

Hey,

I'm currently working on a research project for a Masters degree. The idea is to implement an adaptive control algorithm using a BLDC motor.

I was just wondering if this kit can control this motor:

https://hobbyking.com/en_us/turnigy-sk8-6354-200kv-sensored-brushless-motor-14p.html

Thanks for taking the time.

Dean.

  • The kit can be used to design and debug the control algorithm for this, even run up to high speed with a full load in a short time, but it's not recommended to run with maximum power/current in a long time since the limitation of current output and heat dissipation of the kit need to be considered.