This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28M36P63C2: Output buffer strength

Part Number: F28M36P63C2

The questions below are with reference to the device data sheet

SPRS825E –OCTOBER 2012–REVISED DECEMBER 2017

 

There seems to be conflicting information in the following two parts of the data sheet:

 

Chapter 4.2 column “Output buffer strength” of the table

Here it is stated that the following GPIO numbers has higher than 4 mA drive strength, most with 6 mA and a few with 8 mA:

21, 22, 23, 47, 60-62, 196, 199

 

Chapter 5.5 in note (2) below the table

Here it is stated that the following GPIO has a drive strength of 8 mA:

PD3_GPIO19, PE2_GPIO26, PE3_GPIO27, PH6_GPIO54, PH7_GPIO55, EMU0, TDO, EMU1, PD0_GPIO16, AIO7, AIO4.

 

Which information is correct?