Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE, CONTROLSUITE
Hello,
For our large project we decided to use TMS320F28379D MCU
We bought several Launch Pads and several development boards.
The issue now is ease of connectivity during the long development stage.
On one hand the launch pad provides clean way to connect to the MCU pin. However, we cannot access every pin of the MCU, which is something we need to do.
On the other hand, the development board allows us to access each pin of the MCU via the docking station baseboard. However we cannot find proper multi-pin connector to connect to the pins of that docking station. Without connectors the result is a mess of wires.
Are you able to advise us of connector(s) model number that can be connect to the pins of the docking station base board or be soldered to that docking station base board?
Picture if available would be great.
Regards
Sam