This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TMS320F28377D: stack overflow

Part Number: TMS320F28377D

Tool/software: TI C/C++ Compiler

TMS32F283779D_에러상황.zipI have a question when i testing tms320f28377d

i think stack overflow occured, but i don't know what make this.

next file is  cmd_linker file


MEMORY
{
PAGE 0 :  /* Program Memory */
          /* Memory (RAM/FLASH) blocks can be moved to PAGE1 for data allocation */
          /* BEGIN is used for the "boot to Flash" bootloader mode   */
   BEGIN            : origin = 0x080000, length = 0x000002
   RAMM0            : origin = 0x000122, length = 0x0002DE
   RAMD0            : origin = 0x00B000, length = 0x000800
   RAMLS0           : origin = 0x008000, length = 0x000800
   RAMLS1           : origin = 0x008800, length = 0x000800
   RAMLS2        : origin = 0x009000, length = 0x000800
   RAMLS3        : origin = 0x009800, length = 0x000800
   RAMLS4        : origin = 0x00A000, length = 0x000800
   RAMGS14          : origin = 0x01A000, length = 0x001000     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
   RAMGS15          : origin = 0x01B000, length = 0x001000     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
   RESET            : origin = 0x3FFFC0, length = 0x000002
   /* Flash sectors */
   FLASHA           : origin = 0x080002, length = 0x001FFE /* on-chip Flash */
   FLASHB           : origin = 0x082000, length = 0x002000 /* on-chip Flash */
   FLASHC           : origin = 0x084000, length = 0x002000 /* on-chip Flash */
   FLASHD           : origin = 0x086000, length = 0x002000 /* on-chip Flash */
   FLASHE           : origin = 0x088000, length = 0x008000 /* on-chip Flash */
   FLASHF           : origin = 0x090000, length = 0x008000 /* on-chip Flash */
   FLASHG           : origin = 0x098000, length = 0x008000 /* on-chip Flash */
   FLASHH           : origin = 0x0A0000, length = 0x008000 /* on-chip Flash */
   FLASHI           : origin = 0x0A8000, length = 0x008000 /* on-chip Flash */
   FLASHJ           : origin = 0x0B0000, length = 0x008000 /* on-chip Flash */
   FLASHK           : origin = 0x0B8000, length = 0x002000 /* on-chip Flash */
   FLASHL           : origin = 0x0BA000, length = 0x002000 /* on-chip Flash */
   FLASHM           : origin = 0x0BC000, length = 0x002000 /* on-chip Flash */
   FLASHN           : origin = 0x0BE000, length = 0x002000 /* on-chip Flash */
PAGE 1 : /* Data Memory */
         /* Memory (RAM/FLASH) blocks can be moved to PAGE0 for program allocation */
   BOOT_RSVD       : origin = 0x000002, length = 0x000120     /* Part of M0, BOOT rom will use this for stack */
   RAMM1           : origin = 0x000400, length = 0x000400     /* on-chip RAM block M1 */
   RAMD1           : origin = 0x00B800, length = 0x000800
   RAMLS5      : origin = 0x00A800, length = 0x000800
   RAMGS0      : origin = 0x00C000, length = 0x004000
   RAMGS1      : origin = 0x010000, length = 0x000800
   RAMGS2      : origin = 0x010800, length = 0x000800
   RAMGS3      : origin = 0x011000, length = 0x000800
   RAMGS4      : origin = 0x011800, length = 0x000800
   RAMGS5      : origin = 0x012000, length = 0x000800
   RAMGS6      : origin = 0x012800, length = 0x000800
   RAMGS7      : origin = 0x013000, length = 0x001000
   RAMGS8      : origin = 0x014000, length = 0x001000
   RAMGS9      : origin = 0x015000, length = 0x001000
   RAMGS10     : origin = 0x016000, length = 0x001000
   RAMGS11     : origin = 0x017000, length = 0x001000
   RAMGS12     : origin = 0x018000, length = 0x001000     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
   RAMGS13     : origin = 0x019000, length = 0x001000     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
   CPU2TOCPU1RAM   : origin = 0x03F800, length = 0x000400
   CPU1TOCPU2RAM   : origin = 0x03FC00, length = 0x000400
}
SECTIONS
{
   /* Allocate program areas: */
   .cinit              : > FLASHB      PAGE = 0, ALIGN(4)
   .pinit              : > FLASHB,     PAGE = 0, ALIGN(4)
   .text               : >> FLASHB | FLASHC | FLASHD | FLASHE      PAGE = 0, ALIGN(4)
   codestart           : > BEGIN       PAGE = 0, ALIGN(4)
   /* Allocate uninitalized data sections: */
   .stack              : > RAMM1        PAGE = 1
   .ebss               : >> RAMLS5 | RAMGS0 | RAMGS1       PAGE = 1
   .esysmem            : > RAMLS5       PAGE = 1
   /* Initalized sections go in Flash */
   .econst             : >> FLASHF | FLASHG | FLASHH      PAGE = 0, ALIGN(4)
   .switch             : > FLASHB      PAGE = 0, ALIGN(4)
   .reset              : > RESET,     PAGE = 0, TYPE = DSECT /* not used, */
   Filter_RegsFile     : > RAMGS0,    PAGE = 1
   SHARERAMGS0  : > RAMGS0,  PAGE = 1
   SHARERAMGS1  : > RAMGS1,  PAGE = 1
   ramgs0           : > RAMGS0,     PAGE = 1
   ramgs1           : > RAMGS1,     PAGE = 1
#ifdef __TI_COMPILER_VERSION__
 #if __TI_COMPILER_VERSION__ >= 15009000
 .TI.ramfunc : {} LOAD = FLASHD,
       RUN = RAMLS0 | RAMLS1 | RAMLS2 |RAMLS3,
                         LOAD_START(_RamfuncsLoadStart),
                         LOAD_SIZE(_RamfuncsLoadSize),
                         LOAD_END(_RamfuncsLoadEnd),
                         RUN_START(_RamfuncsRunStart),
                         RUN_SIZE(_RamfuncsRunSize),
                         RUN_END(_RamfuncsRunEnd),
       PAGE = 0, ALIGN(4)
 #else
   ramfuncs            : LOAD = FLASHD,
                         RUN = RAMLS0 | RAMLS1 | RAMLS2 |RAMLS3,
                         LOAD_START(_RamfuncsLoadStart),
                         LOAD_SIZE(_RamfuncsLoadSize),
                         LOAD_END(_RamfuncsLoadEnd),
                         RUN_START(_RamfuncsRunStart),
                         RUN_SIZE(_RamfuncsRunSize),
                         RUN_END(_RamfuncsRunEnd),
                         PAGE = 0, ALIGN(4)   
    #endif
#endif
   /* The following section definitions are required when using the IPC API Drivers */
    GROUP : > CPU1TOCPU2RAM, PAGE = 1
    {
        PUTBUFFER
        PUTWRITEIDX
        GETREADIDX
    }
    GROUP : > CPU2TOCPU1RAM, PAGE = 1
    {
        GETBUFFER :    TYPE = DSECT
        GETWRITEIDX :  TYPE = DSECT
        PUTREADIDX :   TYPE = DSECT
    }
   /* The following section definition are for SDFM examples */
   Filter1_RegsFile : > RAMGS1, PAGE = 1, fill=0x1111
   Filter2_RegsFile : > RAMGS2, PAGE = 1, fill=0x2222
   Filter3_RegsFile : > RAMGS3, PAGE = 1, fill=0x3333
   Filter4_RegsFile : > RAMGS4, PAGE = 1, fill=0x4444
   Difference_RegsFile : >RAMGS5,  PAGE = 1, fill=0x3333
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/