Part Number: TMS320F280049
Other Parts Discussed in Thread: TIDM-HV-1PH-DCAC
Hi experts,
I am working on a project based on TIDM-HV-1PH-DCAC.
To sample the output voltage, I configured ADC following the example code:
Under this configuration, I believe I am using an internal reference which is 3.3V.
In our sampling circuit, we have a 1.65V offset. So, if the output voltage is 0, I should be able to see a ADC result which is 2048.
However, the sampling result offset is always 1024.
If the reference is configured to be 2.5, I believe I should have a result of 2703.
Why I am always getting 1024? Where should I try to find the mistake?
BTW: The offset in PPB is 0.
Thanks!