Part Number: TMDSHVMTRINSPIN
Other Parts Discussed in Thread: CONTROLSUITE
Tool/software: Code Composer Studio
Hi all,
Good Afternoon to all of u,
I am working for Cybermotion Technology Pvt Ltd Hyderabad (India) , as Embedded Software Engineer, we are very happy to share that we are sold 10000+ nos controller for Solar Water Pump Controller(Variable Frequency Drive) using your TIVA C Series (TM4C123GH6PGE) to run 3 ph Induction Motor.In this project, we use all possible technique that we got through your portal.The concept is based on SVPWM to generated Pulses and V/F method for Speed Control.
Right now,we are working to control BLDC and PMSM Motor.(3 Hp and 5 Hp rating) For that we already brought TMS320C2000 (TMDSHVMTRINSPIN) Development Tools from Ti i.e for 200 watt or 400 watt BLDC and PMSM Motor.So,this is completely GUI based to operate the Motor.Here we are only able to Control the external Parameters such as speed and some Current Limits. So,this GUI automatically synchronize with the motor and Control according to motor Selection (BLDC,PMSM) . Here's our worries is that, we are unable to see the internal mechanism and how algorithm are working because there is no reference Code. Now we are in blind mode what to do how to do because that is totally depends on GUI Application.
This Kit is not support for 3 Hp and 5 Hp PMSM and BLDC Motor but software we can use directly with some few modification such as motor parameters , Current Settings, speed ,voltage,etc..
For this we need actual Source file(C programming Code) or any reference code by which we start our work easily. We are ready with hardware and we looking for software from u.
Please help us and we are always depends on your Technology and products
Thank you!