Part Number: TMS320F280049
All:
I know on the F2837x, the ADCs all share ADC14 and ADC15,
On the F28004x, I am using an external 3 volt reference for ADCA, ADCB, and ADCC.
Question:
If I use A0/B15/C15 input to measure a fixed voltage (in our case 2.5 volts), can I read the value on ADCA without having to deselect B15 and C15?
Ideally, I would like to set up all 3 ADCs and input the fixed voltage without having to "deselect" - is that possible? (and am I making sense?)