This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28379D: Input Under shoot and Over shoot capability

Part Number: LAUNCHXL-F28379D

Hello Every One,

I'm Using LAUNCHXL-F28379D for my application. I have a digital Input to the Launchxl which is indicated in yellow color in the attached two images (Oscilloscope images). Please tell me if this much of an Under shoot is a problem or not. ?
peak under shoot is about 620mV and time taken to come back to zero is 10nS as in image 2.

Thank you and best regards,

Thilesh De Silva.