Other Parts Discussed in Thread: C2000WARE
Hello,
I am trying to get the USB communication of a TMS320F28377D Dual-Core Delfino ™ via a virtual COM port. I downloaded the C2000WARE_1.00.06.00 and installed the windows driver. The COM port appears in the device manager with the name TivaWare USB serial port (COM18). So far everything is fine.
Communication with 9.6kBaud is possible. But other baud rates will not work except with the Multi Threaded TTY Terminal (MTTTY255). Further attempts were made with Hammer Term (HTerm) and LabView NI VISA Runtime 5.4. For the last both only the 9.6kBaud works.
 Under Linux all baud rates are working well, which is why I suspect the Windows driver here. Does anyone have recommendations to get all baudrates? The final goal is to run communication via LabView (NI VISA).
Kind regards,
Gundolf