Part Number: TMS320F28379D
Tool/software: Code Composer Studio
Dear support,
I run two examples: spi_loopback_cpu1 and spi_loopback_dma_cpu1.
In both examples I removed loopback . In spi_loopback_dma_cpu1 I added calling InitSpiGpio() send/read data always:
while(1)
{
StartDMACH6();
StartDMACH5();
}
In the 1st example in see all signals good(1-SPISTEA, 2-SPICLKA, 3-SPISIMOA)
In the 2nd example with DMA I don't see SPISTEA signal and see SPICLKA always
May be I do something wrong? Should I see SPISTEA signal too? We would like to communicate with FPGA via SPI . I think to do it via DMA , but we can not work without SPISTEA signal.
Thanks,Sabina