This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMDSSOLARPEXPKIT: Vboost detected by Multimeter and command window display is not the same

Part Number: TMDSSOLARPEXPKIT

Tool/software: Code Composer Studio

Hi, I have some problems with solar explorer Kit. When i test the kit, I found that the value of Vboost detected by Multimeter  and command window display is not the same,

At the build 2,if Vboost >30V,enable inverter closed loop operation.However,when it rises up  to 36V, command window display under 20V, which lead to unwork of kit.

Can you help me? Thank you.