Part Number: TMS320F28335
Hello
I am having problems with the SoC from EPwm1A and B. I am triggering a SoC on CTR= 0 for SOCA and CTR=TPCTR for SOCB. The results are periodic bad readings on both ADCINA3/B3 at the same instance in time. When I only enable SoC on CTR=0 SOCA (or CTR=TPCTR SOCB), i.e. half the frequency, all results are ok. I have also tried trigging off of EPwm2 SOCA CTR=TPCTR (instead of EPwm1B) still get bad results.
I have adjusted the timing, slowed down the ISR loop, but get the same results.
Any help/suggestions would be appreciated
Thank
John
I have broken my code in 4 sections
1) EPWM Config
2) ADC Config
3) Main
4) Interrupts
My EPWMs are setup as follows:
// EPWM Module 1 config
EPwm1Regs.TBPRD = PWM1_TIMER_TBPRD; //
EPwm1Regs.TBPHS.half.TBPHS = 0; // Set Phase register to zero
EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Symmetrical mode
EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Master module
EPwm1Regs.TBCTL.bit.PRDLD = TB_SHADOW;
EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_CTR_ZERO; // Sync down-stream module
EPwm1Regs.TBCTL.bit.CLKDIV = 0x0000; // /1 TBCLK=SYSCLKOUT/(HSPCLKDIV*CLKDIV)
EPwm1Regs.TBCTL.bit.HSPCLKDIV = 0x0000; //1 TBCLK=SYSCLKOUT/(HSPCLKDIV*CLKDIV)
EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
EPwm1Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // load on CTR=Zero
EPwm1Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO; // load on CTR=Zero
EPwm1Regs.AQCTLA.bit.CAU = AQ_SET; // set actions for EPWM1A
EPwm1Regs.AQCTLA.bit.CAD = AQ_CLEAR;
EPwm1Regs.DBCTL.bit.IN_MODE = 0x00; // EPWM1A Source, thus do not need AQCTLB Configured
EPwm1Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE; // enable Dead-band module
EPwm1Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC; // Active Hi complementary
EPwm1Regs.DBFED = 50; // FED = 50 TBCLKs
EPwm1Regs.DBRED = 50; // RED = 50 TBCLKs
EALLOW;
// EPwm1Regs.TZCTL.bit.TZA = 1; // Forced high
// EPwm1Regs.TZCTL.bit.TZB = 1; // Forcec high
// EPwm1Regs.TZEINT.bit.CBC = 0; // No Interrupt for One-Shot
// EPwm1Regs.TZEINT.bit.OST = 0; // No Interrupt for Cycle to Cycle
// EPwm1Regs.TZSEL.all = 0; // No HW trip signal
EDIS;
EPwm1Regs.ETSEL.bit.SOCAEN = 1; // Enable SOCA (Bit11)
EPwm1Regs.ETSEL.bit.SOCASEL = 0x1; // SOC A Pulse generate when TPCTR = 0;
EPwm1Regs.ETPS.bit.SOCAPRD = 1; // Generate pulse on 1st event
EPwm1Regs.ETSEL.bit.SOCBEN = 1; // Enable SOCB (Bit11)
EPwm1Regs.ETSEL.bit.SOCBSEL = 0x2; // SOC B Pulse generate when TPCTR = 0;
EPwm1Regs.ETPS.bit.SOCBPRD = 1; // Generate pulse on 1st event
EPwm1Regs.ETSEL.bit.INTSEL = 1; //ET_CTR_ZERO;
EPwm1Regs.ETSEL.bit.INTEN = PWM1_INT_ENABLE; // Enable INT
EPwm1Regs.ETPS.bit.INTPRD = ET_1ST; // Generate INT on 1st event
// EPWM Module 2 config
EPwm2Regs.TBPRD = PWM1_TIMER_TBPRD; // Period
EPwm2Regs.TBPHS.half.TBPHS = 0; // Set Phase register to zero
EPwm2Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Symmetrical mode
EPwm2Regs.TBCTL.bit.PHSEN = TB_ENABLE; // Slave module
EPwm2Regs.TBCTL.bit.PRDLD = TB_SHADOW;
EPwm2Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN; // sync flow-through
EPwm2Regs.TBCTL.bit.CLKDIV = 0x0000; // /1 TBCLK=SYSCLKOUT/(HSPCLKDIV*CLKDIV)
EPwm2Regs.TBCTL.bit.HSPCLKDIV = 0x0000; //1 TBCLK=SYSCLKOUT/(HSPCLKDIV*CLKDIV)
EPwm2Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
EPwm2Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
EPwm2Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // load on CTR=Zero
EPwm2Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO; // load on CTR=Zero
EPwm2Regs.AQCTLA.bit.CAU = AQ_SET; // set actions for EPWM2A
EPwm2Regs.AQCTLA.bit.CAD = AQ_CLEAR;
EPwm2Regs.DBCTL.bit.IN_MODE = 0x00; // EPWM2A Source
EPwm2Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE; // enable Dead-band module
EPwm2Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC; // Active Hi complementary
EPwm2Regs.DBFED = 50; // FED = 50 TBCLKs
EPwm2Regs.DBRED = 50; // RED = 50 TBCLKs
EALLOW;
EPwm2Regs.TZCTL.bit.TZA = 1; // Forced high
EPwm2Regs.TZCTL.bit.TZB = 1; // Forcec high
EPwm2Regs.TZEINT.bit.CBC = 0; // No Interrupt for One-Shot
EPwm2Regs.TZEINT.bit.OST = 0; // No Interrupt for Cycle to Cycle
EPwm2Regs.TZSEL.all = 0; // No HW trip signal
EDIS;
// EPwm2Regs.ETSEL.bit.SOCAEN = 1; // Enable SOCA (Bit11)
// EPwm2Regs.ETSEL.bit.SOCASEL = 0x2; // SOC A Pulse generate when TPCTR = TPRD;
// EPwm2Regs.ETPS.bit.SOCAPRD = 1; // Generate pulse on 1st event
My ADC is configured as followed:
// Configure ADC
EALLOW;
SysCtrlRegs.PCLKCR0.bit.ADCENCLK = 1;
// ADC_cal();
EDIS;
//ADCTRL3
AdcRegs.ADCREFSEL.bit.REF_SEL = 0x0; // Voltage Reference ? assuming internal
AdcRegs.ADCTRL3.bit.ADCBGRFDN = 0x3; // Power up bandgap/reference/ADC circuits
AdcRegs.ADCTRL3.bit.ADCPWDN = 0x1; // Power up bandgap/reference/ADC circuits
AdcRegs.ADCTRL3.bit.ADCCLKPS = 0x0; //HSPCLK passed thru
AdcRegs.ADCTRL3.bit.SMODE_SEL = 0x1; // 1)Simultaneous sampling mode 0)Sequential
DELAY_US(ADC_usDELAY); // Delay before converting ADC channels
//ADCTRL1
AdcRegs.ADCTRL1.bit.SUSMOD = 0x0;
AdcRegs.ADCTRL1.bit.ACQ_PS = 0x8; //Acq window size: ("6"+1)xADClk period 7*1/(75e6/2)=183ns
AdcRegs.ADCTRL1.bit.CPS = 0x1; // 0=>ADCLK=HSPCLK/2 (1=>ADCLK=HSPCLK/2)
AdcRegs.ADCTRL1.bit.CONT_RUN = 0x0;
AdcRegs.ADCTRL1.bit.SEQ_OVRD = 0x0;
AdcRegs.ADCTRL1.bit.SEQ_CASC = 0x1; //
//ADCTRL1
AdcRegs.ADCTRL2.bit.EPWM_SOCA_SEQ1 = 0x1;// Enable SOCA from ePWM to start SEQ1
AdcRegs.ADCTRL2.bit.EPWM_SOCB_SEQ= 0x1;// Enable SOCA from ePWM to start SEQ1
AdcRegs.ADCTRL2.bit.INT_ENA_SEQ1 = 0x1; // Enable SEQ1 interrupt (every EOS)
//==
AdcRegs.ADCMAXCONV.all = 0x0006; //4 double conv's sequencer
AdcRegs.ADCCHSELSEQ1.bit.CONV00 = 0x0; //0,1 Setup ADCINA0/B0
AdcRegs.ADCCHSELSEQ1.bit.CONV01 = 0x0; //2,3 Setup ADCINA0/B0
AdcRegs.ADCCHSELSEQ1.bit.CONV02 = 0x1; //4,5 Setup ADCINA1/B1
AdcRegs.ADCCHSELSEQ1.bit.CONV03 = 0x2; //6,7 Setup ADCINA2/B2
AdcRegs.ADCCHSELSEQ2.bit.CONV04 = 0x3; //8,9 Setup ADCINA3/B3
AdcRegs.ADCCHSELSEQ2.bit.CONV05 = 0x0; //10,11 Setup ADCINA0/B0
AdcRegs.ADCCHSELSEQ2.bit.CONV06 = 0x3; //12,13 Setup ADCINA3/B
My Main
#pragma CODE_SECTION(epwm1_timer_isr, "ramfuncs");
#pragma CODE_SECTION(adc_isr, "ramfuncs");
#pragma CODE_SECTION(CpuTimer1_int13_isr, "ramfuncs");
#pragma CODE_SECTION(FOC_Update, "ramfuncs");
#pragma CODE_SECTION(ADC_ResultSave, "ramfuncs");
#pragma CODE_SECTION(ADC_ResultUpdate, "ramfuncs");
#pragma CODE_SECTION(commo_routine, "ramfuncs");
main(void)
{
InitSysCtrl();
DisableDog();
DINT;// Disable CPU interrupts
InitPieCtrl();
IER = 0x0000;
IFR = 0x0000;
InitPieVectTable();
EALLOW; // This is needed to write to EALLOW protected registers
PieVectTable.EPWM1_INT = &epwm1_timer_isr;
PieVectTable.ADCINT = &adc_isr;
PieVectTable.XINT13 = &CpuTimer1_int13_isr; // CPU1 32bit Timer INT13
EDIS;
EALLOW;
XIntruptRegs.XNMICTR = 0; //Counter (CPU_Timer1 = INT13)
EDIS;
MemCopy(&RamfuncsLoadStart, &RamfuncsLoadEnd, &RamfuncsRunStart);
InitFlash();
EPwm1TimerIntCount = 0;
MainLoopCount = 0;
IER |= M_INT1 | M_INT3 | M_INT13; //CPU Interrupt 13 (CPUTimer1) and 3(ePWM1): Need to set IFR and IER
PieCtrlRegs.PIEIER3.bit.INTx1 = 1; // ePWM1_INT_ENABLE (ePWM1)
PieCtrlRegs.PIEIER1.bit.INTx6 = 1;
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM
//========= Application intialization =================
//====================================================
//=== Put the Flash to sleep ========
// EALLOW;
// FlashRegs.FPWR.bit.PWR = FLASH_SLEEP;
//=================================
// FlashRegs.FPWR.bit.PWR = FLASH_SLEEP;
// EDIS;
//=============== State Machine ====================
State = 1;
while(1)
{
if(commo_flag)
{ commo_flag = 0;
commo_routine();
}
if(adc_flag)
{
adc_flag = 0;
ADC_ResultUpdate();
//ADC_VdcMotorTmpUpdate();
//CurrentPeakUpdate();
}
if(foc_flag)
{
foc_flag = 0;
FOC_Update();
}
switch(State)
{
case 1:
Initial_Configure();
break;
case 2:
Initial_Loop();
break;
case 3:
Run_Configure();
break;
case 4:
Run_Loop();
break;
case 5:
Fault_Loop();
break;
case 6:
EEPROMB_Loop();
break;
}
MainLoopCount++;
}
}
MY Interupts
interrupt void CpuTimer1_int13_isr(void) // CPU1 32bit Timer INT13
{
commo_flag = 1; //change 10aug2018
CpuTimer1Regs.TCR.bit.TIF = 1; //change 10aug2018
PieCtrlRegs.PIEACK.all = PIEACK_GROUP3; //change 10aug2018
}
interrupt void adc_isr(void)
{
// EPwm1Regs.ETSEL.bit.SOCAEN = 0; // Disable SOCA (Bit11)
// EPwm1Regs.ETSEL.bit.SOCBEN = 0; // Disable SOCA (Bit11)
ADCCount++; //For Testing
ADC_ResultSave();
adc_flag = 1;
EPwm1Regs.ETCLR.bit.SOCA = 1;// Clears ETFLG[SOCA] Flag
EPwm1Regs.ETCLR.bit.SOCB = 1;// Clears ETFLG[SOCA] Flag
EPwm1Regs.ETCLR.bit.INT= 1;// Clears ETFLG[SOCA] Flag
// EPwm2Regs.ETCLR.bit.SOCA = 1;// Clears ETFLG[SOCA] Flag
// EPwm1Regs.ETSEL.bit.SOCAEN = 1; // Enable SOCA (Bit11)
// EPwm2Regs.ETSEL.bit.SOCAEN = 1; // Enable SOCA (Bit11)
AdcRegs.ADCTRL2.bit.RST_SEQ1 = 1; // Reset SEQ1
//AdcRegs.ADCTRL2.bit. = 1; // Reset SEQ1
AdcRegs.ADCST.bit.INT_SEQ1_CLR = 1; // Clear INT SEQ1 bit
//AdcRegs.ADCST.bit.INT_SEQ2_CLR = 1;
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
}
interrupt void epwm1_timer_isr(void)
{
EPwm1TimerIntCount++;
FOC_Update();
foc_flag = 1;
EPwm1Regs.ETCLR.bit.INT = 1;
PieCtrlRegs.PIEACK.all = PIEACK_GROUP3;
}