Tool/software: Code Composer Studio
Hello,
I'm trying to use either CCS or Simulink to read a quadrature encoder via eQEP and I am trying to use the headers on the f28379d launchpad that are labeled as QEP-A. The default pin assignments in the control suite project "eqep_pos_speed_cpu01" are GPIO 20-23. However, there is no map for these headers to their GPIO assignments in any of the manuals relating to the launchpad (there is no mapping in the cpu manual, the f28379d, or even the users guide).
What GPIO pins does the QEP-A pin row (J14) correspond to? I tried connecting a quadrature encoder according to the attached diagram I found in the user guide and using Simulink (with these pin assignments) to program eQEP-A, but it was only returning the number 17 for some reason.
Any help you can provide would be greatly appreciated.
Thanks,
Tyler A