Part Number: TMS320F2808
Hello:
The problem is described as follows:
DSP2808 83 pin (GPIO24), 3K resistance pull-down, and power on 200ms of DSP reset time, 83 pin outputs a square wave signal, as shown in the figure:
Different control panel DSP output level is not the same, some DSP output level below 0.5v, some output more than 3V, hardware, software version is the same;
Question: 1. Why there is such a big difference in the high level of DSP pin in the reset state;
2. What is the internal structure of GPIO24? Is it equivalent to pulling up a resistance?
Best Regards
Leon
文晔集团
广东省深圳市南山区高新中三道9号环球数码大厦12楼
Mobile:(86)159 8985 2994
Tel:(86)755-26743880 Ext:6643
Fax:(86)755-26743990