Part Number: TMS320F28069
Tool/software: Code Composer Studio
Hi,
I'm trying to implement i2c master operation with an EEPROM (M24LR16E-R). Because I didn't find any example code with i2c FIFO interrupts, I coded it by reference manual.
But now I have a problem with writing data to EEPROM. Reading is working fine with EEPROM, as I can see with a scope.
With this EEPROM, I can only write 4 bytes of data every 5 ms to it. So It is very simple, when writing 4 bytes to EEPROM, I set I2CCNT to 6 (2 address bytes + 4 data bytes), and set FIFO level to 0 and start the i2c as transmitter. Then I would expect, that FIFO interrupt is occurring after 4 bytes written (2 address bytes, 2 data bytes). In FIFO interrupt I copy the last 2 bytes to I2CDXR register. After writing last 2 bytes, I should get the the stop condition detected interrupt, because 6 bytes are written (I2CCNT was set to 6).
Watching the signals with a scope gives me another behaviour. Here is a screenshot of the scope:
The yellow signal is i2c_int1a interrupt occurring, red is i2c_int2a interrupt (fifo), blue is SCL and green is SDA. Yellow and red signals are just GPIO toggles at entrance of interrupt.
As you can see, FIFO interrupt (i2c_int2a) occurres after 3 bytes written (without I2C slave address of EEPROM). As I said, in FIFO interrupt I write only 2 new bytes to I2CDXR register, but after FIFO interrupt, 3 bytes are written, then the stop condition detected interrupt is occurring (yellow). So the correct 4 bytes (containing 0, 1, 2, 3) are written to the correct address (0) of EEPROM, but the behaviour of FIFO interrupt is not as I expect.
My question is now, does the i2c slave address counts to the number of bytes that fifo has to write or not? For I2CCNT register the slave address does not count, I set it to 6 and 6 bytes are written (without i2c slave address). But I would expect, that FIFO interrupt would occur after 4 bytes and not after 3 bytes.
When I set a breakpoint in FIFO interrupt, before writing new data to I2CDXR register, the correct number of bytes are written, as you can see:
but interrupt is occurring before last byte is sent. Is that the normal behyviour?
Thanks for any help.
Regards,
Dani