Hi,
I've been looking at the TINA files which show the "bleed" phenomenon where a large external capacitor will exhibit voltage drift if the external resistor's value is too high.
Namely I found two different TINA files :
In my case I'm working with a TMS320F28379D and I have several signals for which I need to make a trade-off between sample rate, accuracy, bandwidth, etc.
Hence the following question: where can I find an "official" model of the internal discharge of the ADC?
- In ADCChargeShareSampleRate.TSC it is modeled as a 10ns discharge into a 0V source through 1Ohm, repeated at 80kHz
- In PiccoloSampleRate_settling.TSC it is modeled as a 200ns charge to a 3.3V source through 1Ohm, repeated at 100Hz.
These two models seem to be quite different, so I don't know how to interpret this information.
Cheers,
Pierre