This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377S: F2837xS support library v2.10 provided in the controlSUITE package

Part Number: TMS320F28377S
Other Parts Discussed in Thread: CONTROLSUITE,

Hello,

I have a question on the F2837xS support library v2.10 provided in the controlSUITE package.

In particular, I am now exploring the function of the CLA module on the TMS320F28377S device.

With reference to the project of cla_matrix_mpy, the function of CLA_runTest() listed in the file of cla_matrix_mpy_cpu01.c  calls the following function: Cla1ForceTask1andWait().

It seems that the Cla1ForceTask1andWait() function is provided by some library.

And it seems that this function starts the __interrupt void Cla1Task1() listed in the file of matrix_mpy.cla and waits till the Cla1Task1() ends its routine.

Is this Cla1ForceTask1andWait() function the only way to call the CLA processing?

Thank you for yuor guidance.

With regards,

G. Kim