Part Number: TMS320F28379S
I am running 2 SCI buses, B and C on the TMS320F28379. When running the board, both have the same settings, shown below:
// configure SCICCR for SCI-C
ScicRegs.SCICCR.bit.STOPBITS = 0; // 1 stop bit
ScicRegs.SCICCR.bit.PARITY = 0; // odd parity
ScicRegs.SCICCR.bit.PARITYENA = 0; // parity disabled
ScicRegs.SCICCR.bit.LOOPBKENA = 0; // loopback disabled
ScicRegs.SCICCR.bit.ADDRIDLE_MODE = 0; // idle-line mode protocol selected
ScicRegs.SCICCR.bit.SCICHAR = 7; // 8 data bits
// configure SCICTL1 for SCI-C
ScicRegs.SCICTL1.bit.RXERRINTENA = 0; // receive error interrupt disabled
ScicRegs.SCICTL1.bit.SWRESET = 0; // software reset enabled (active low) while configuring
ScicRegs.SCICTL1.bit.TXWAKE = 0; // SCI TX Wake feature disabled
ScicRegs.SCICTL1.bit.SLEEP = 1; // Sleep mode enabled
ScicRegs.SCICTL1.bit.TXENA = 1; // enable TX
ScicRegs.SCICTL1.bit.RXENA = 1; // enable RX
// configure SCICTL2 for SCI-C
ScicRegs.SCICTL2.bit.RXBKINTENA = 1; // enable receiver-buffer/break interrupt
ScicRegs.SCICTL2.bit.TXINTENA = 0; // disable TX ready interrupt
// configure SCIHBAUD & SCILBAUD for SCI-C
Uint16 brr = 64;// = (Uint16) round(LSPCLK / (SCIC_RS485_BAUD_RATE * 8.0) - 1);
ScicRegs.SCIHBAUD.all = brr >> 8; // Baud Rate = 125k
ScicRegs.SCILBAUD.all = brr & 0xFF; // Baud Rate = 125k
// configure SCIFFTX for SCI-C
ScicRegs.SCIFFTX.bit.SCIRST = 1; // SCI FIFO can resume transmit and receive
ScicRegs.SCIFFTX.bit.SCIFFENA = 1; // SCI FIFO enhancements are enabled
ScicRegs.SCIFFTX.bit.TXFIFORESET = 0; // Reset the TX FIFO pointer to zero and hold in reset while configuring
ScicRegs.SCIFFTX.bit.TXFFIENA = 0; // disable transmit FIFO interrupts
ScicRegs.SCIFFTX.bit.TXFFIL = 0; // set transmit FIFO interrupt level bits to 0
// configure SCIFFRX for SCI-C
ScicRegs.SCIFFRX.bit.RXFIFORESET = 0; // Reset the RX FIFO pointer to zero and hold in reset while configuring
ScicRegs.SCIFFRX.bit.RXFFIENA = 1; // Receive FIFO interrupt enable
ScicRegs.SCIFFRX.bit.RXFFIL = 1; // Set receive FIFO interrupt levels bit to 1
// configure SCIFFCT for SCI-C
ScicRegs.SCIFFCT.bit.CDC = 0; // disable auto-baud alignment
ScicRegs.SCIFFCT.bit.FFTXDLY = 0; // set FIFO transfer delay to 0
// Relinquish SCI from Reset
ScicRegs.SCICTL1.bit.SWRESET = 1; // disable software reset
ScicRegs.SCIFFTX.bit.TXFIFORESET = 1; // disable TX FIFO reset
ScicRegs.SCIFFRX.bit.RXFIFORESET = 1; // disable RX FIFO reset
With the same thing on SCIB.
SCIB works appropriately, however I cannot detect any activity with SCIC. This is because after some amount of time the status error flag goes high for BRKDT.
This occurs again if I do a SWRESET on the device, and continues to do so.
The error occurs even if no input is being applied and the RX line is continuously low.
What exactly does this error mean in this case?