This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049C: Driverlib I2C MPU6050 Help

Part Number: TMS320F280049C

Hi everyone,

I am working on a project in which I need to poll an accelerometer for motion data, however, I am running into trouble when I try to adapt the example code provided in the DriverLib documentation to my problem. When I hooked up my development board to an oscilliscope, I notice the following behaviour:

C2000: Writes address of MPU to I2C Bus

MPU: No ACK

The code below is trying to request and read back a single register address of the MPU-6050. I have attached the documentation pdf below if you would like to review it. The protocol in question is on page 34.

#include "driverlib.h"
#include <device.h>
#include <stdint.h>

#define WHO_AM_I        0x75
#define MPU_ADDRESS     0x68

void initI2C();
__interrupt void i2cFIFOISR();

uint16_t mpu_data;
uint16_t status;

void main() {
	/* Setup C2000 */
	Device_init();
	Device_initGPIO();

    /* Setup GPIO for I2C */
    GPIO_setPinConfig(GPIO_35_SDAA);
    GPIO_setPadConfig(35U, GPIO_PIN_TYPE_PULLUP);
    GPIO_setQualificationMode(35U, GPIO_QUAL_ASYNC);
    GPIO_setPinConfig(GPIO_37_SCLA);
    GPIO_setPadConfig(37U, GPIO_PIN_TYPE_PULLUP);
    GPIO_setQualificationMode(37U, GPIO_QUAL_ASYNC); 

    /* Setup interrupts */
	Interrupt_initModule();
	Interrupt_initVectorTable();
    Interrupt_register(INT_I2CA, &i2cFIFOISR);

    /* Call i2c setup function */
	initI2C();

    /* Enable interrupts system-wide */
    Interrupt_enable(INT_I2CA);
    EINT;
    ERTM;

    I2C_setDataCount(I2CA_BASE, 1);


    while (1) {
        while (I2C_isBusBusy(I2CA_BASE)) {}
        // I2C_putData(I2CA_BASE, WHO_AM_I);
        I2C_setConfig(I2CA_BASE, I2C_MASTER_SEND_MODE);
        I2C_sendStartCondition(I2CA_BASE);
        status = I2C_getStatus(I2CA_BASE);
    }
}

void initI2C() {
	I2C_disableModule(I2CA_BASE);

    /* Configure for 400 kHz clock with a 50% duty cycle */
    I2C_initMaster(I2CA_BASE, DEVICE_SYSCLK_FREQ, 100000, I2C_DUTYCYCLE_33);
    I2C_setBitCount(I2CA_BASE, I2C_BITCOUNT_8);
    I2C_setSlaveAddress(I2CA_BASE, MPU_ADDRESS);
    I2C_setEmulationMode(I2CA_BASE, I2C_EMULATION_FREE_RUN);

    I2C_enableInterrupt(I2CA_BASE, I2C_INT_REG_ACCESS_RDY | I2C_INT_STOP_CONDITION);

    I2C_enableFIFO(I2CA_BASE);
    I2C_clearInterruptStatus(I2CA_BASE, I2C_INT_RXFF | I2C_INT_TXFF);

    I2C_enableModule(I2CA_BASE);
}

__interrupt void i2cFIFOISR() {
    I2C_InterruptSource source;

    source = I2C_getInterruptSource(I2CA_BASE);


    switch (source) {
        case I2C_INTSRC_REG_ACCESS_RDY:

            if((I2C_getStatus(I2CA_BASE) & I2C_STS_NO_ACK) != 0) {
                I2C_sendStopCondition(I2CA_BASE);
                I2C_clearStatus(I2CA_BASE, I2C_STS_NO_ACK);
            }
            
            I2C_setConfig(I2CA_BASE, I2C_MASTER_RECEIVE_MODE);
            I2C_putData(I2CA_BASE, WHO_AM_I);
            I2C_sendStartCondition(I2CA_BASE);
            mpu_data = I2C_getData(I2CA_BASE);
            I2C_sendStopCondition(I2CA_BASE);
            I2C_setConfig(I2CA_BASE, I2C_MASTER_SEND_MODE);
            break;

        case I2C_INTSRC_STOP_CONDITION:
            I2C_sendStopCondition(I2CA_BASE);
            mpu_data = I2C_getData(I2CA_BASE);
            break;

        default:
            mpu_data = I2C_getData(I2CA_BASE);
            I2C_sendNACK(I2CA_BASE);
            break;
    }


    Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP8);
}

Many thanks!MPU-6050_DataSheet_V3 4.pdf

  • Hi Edward,

    Are you probing the I2C bus close to the slave device (MPU) interface? Make sure that the data integrity is good at the slave. Also, make sure the wire-hookup is correct at the slave device, i.e. correct GPIOs, etc.

    Is your MPU slave address set to AD0 (68) or AD1 (69)? If your HW setup is correct and the proper slave address is being received at the slave interface properly (you see the correct addressing on the oscilloscope) then it might be a software config issue on your MPU, since an ACK is not being seen.

    Please provide waveform screenshots at the slave interface if the above does not help fix the issue.

    Best,
    Kevin