Part Number: TMDSHVMTRPFCKIT
Other Parts Discussed in Thread: DRV8301
Dear TI experts:
For the shunt current feedback circuit, I carefully compare both circuits in TMDSHVMTRPFCKIT and DRV8301-HC-C2-KIT.
1. In TMDSHVMTRPFCKIT, the REF3118 is applied to obtain 1.8V, then the offset 1.65 is produced bu the OPA circuit. But the related circuit is much simpler in DRV8301-HC-C2-KIT.
I think TMDSHVMTRPFCKIT's design should be better, but I don't exactly know why? Could you kindly show me?
I think TMDSHVMTRPFCKIT's design should be better, but I don't exactly know why? Could you kindly show me?
2. For the TMDSHVMTRPFCKIT's design, it uses "inverting" amplifier structure. That means Vout=3.3V when Ipeak= -10A, instead of Ipeak= +10A, right? (Note: "non-inverting" amplifier structure in DRV8301-HC-C2-KIT)
3. In the TMDSHVMTRPFCKIT's design, the shunt resistor is 0.02Ohm and the Ipeak is 10A.
If I change the shunt resistor to 0.005Ohm (8W), the Ipeak should be 40A.
If I change the shunt resistor to 0.002Ohm (20W), the Ipeak should be 100A.
For my target application: PMSM, Vbus=86.4V, rated 3KW (peak 7.2KW), could you kindly suggest me how to choose the shunt resistor (including the Watt)?
If I change the shunt resistor to 0.005Ohm (8W), the Ipeak should be 40A.
If I change the shunt resistor to 0.002Ohm (20W), the Ipeak should be 100A.
For my target application: PMSM, Vbus=86.4V, rated 3KW (peak 7.2KW), could you kindly suggest me how to choose the shunt resistor (including the Watt)?
Hope to hear from you soon.
I will appreciate your help so much~
Wish you the best!
Tang Han