This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377D-EP: What is the maximum volume of on-chip flash I can use for single-core application, please?

Part Number: TMS320F28377D-EP

Hi everyone,

I'm wandering the maximum volume of on-chip flash that is available for single-core application.

 *  Per datasheet, the maximum volume of on-chip flash is up to 1M bytes.

 *  From architecture of F28377D, I noticed that the on-chip flash is for different CPU core, 512k bytes for each CPU core.

So that I'm confused.

Is there anyone that knows the maximum available space of on-chip flah for single-core application, please?

Is the flash space connected to core2 available for CPU1 if I only use one CPU core in my application, please? 

Thank you.

Kind regards,

Shawn