Part Number: TMS320F28379D
I am new to the TMS320F28379D ,hence i am running the example programs to understand . i ran the adc_soc_continuous_cpu01.c program from c2000 but the output is unipolar . how do i solve this. the input given is 0.5v and 20khz . i code i have used is given below.
//###########################################################################
//
// FILE: adc_soc_continuous_cpu01.c
//
// TITLE: ADC continuous self-triggering for F2837xD.
//
//! \addtogroup cpu01_example_list
//! <h1> ADC Continuous Triggering (adc_soc_continuous)</h1>
//!
//! This example sets up the ADC to convert continuously, achieving maximum
//! sampling rate.\n
//!
//! After the program runs, the memory will contain:
//!
//! - \b AdcaResults \b: A sequence of analog-to-digital conversion samples
//! from pin A0. The time between samples is the minimum possible based on the
//! ADC speed.
//
//###########################################################################
// $TI Release: F2837xD Support Library v3.05.00.00 $
// $Release Date: Tue Jun 26 03:15:23 CDT 2018 $
// $Copyright:
// Copyright (C) 2013-2018 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without
// modification, are permitted provided that the following conditions
// are met:
//
// Redistributions of source code must retain the above copyright
// notice, this list of conditions and the following disclaimer.
//
// Redistributions in binary form must reproduce the above copyright
// notice, this list of conditions and the following disclaimer in the
// documentation and/or other materials provided with the
// distribution.
//
// Neither the name of Texas Instruments Incorporated nor the names of
// its contributors may be used to endorse or promote products derived
// from this software without specific prior written permission.
//
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//###########################################################################
//
// Included Files
//
#include "F28x_Project.h"
//
// Function Prototypes
//
void ConfigureADC(void);
void SetupADCContinuous(Uint16 channel);
//
// Defines
//
#define RESULTS_BUFFER_SIZE 256 //buffer for storing conversion results
//(size must be multiple of 16)
//
// Globals
//
Uint16 AdcaResults[RESULTS_BUFFER_SIZE];
Uint16 resultsIndex;
void main(void)
{
//
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the F2837xD_SysCtrl.c file.
//
InitSysCtrl();
//
// Step 2. Initialize GPIO:
// This example function is found in the F2837xD_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
//
InitGpio(); // Skipped for this example
//
// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
//
DINT;
//
// Initialize the PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the F2837xD_PieCtrl.c file.
//
InitPieCtrl();
//
// Disable CPU interrupts and clear all CPU interrupt flags:
//
IER = 0x0000;
IFR = 0x0000;
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in F2837xD_DefaultIsr.c.
// This function is found in F2837xD_PieVect.c.
//
InitPieVectTable();
//
// Configure the ADC and power it up
//
ConfigureADC();
//
// Setup the ADC for continuous conversions on channel 0
//
SetupADCContinuous(0);
//
// Enable global Interrupts and higher priority real-time debug events:
//
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM
//
// Initialize results buffer
//
for(resultsIndex = 0; resultsIndex < RESULTS_BUFFER_SIZE; resultsIndex++)
{
AdcaResults[resultsIndex] = 0;
}
resultsIndex = 0;
//
// take conversions indefinitely in loop
//
do
{
//
//enable ADCINT flags
//
EALLOW;
AdcaRegs.ADCINTSEL1N2.bit.INT1E = 1;
AdcaRegs.ADCINTSEL1N2.bit.INT2E = 1;
AdcaRegs.ADCINTSEL3N4.bit.INT3E = 1;
AdcaRegs.ADCINTSEL3N4.bit.INT4E = 1;
AdcaRegs.ADCINTFLGCLR.all = 0x000F;
EDIS;
//
//initialize results index
//
resultsIndex = 0;
//
//software force start SOC0 to SOC7
//
AdcaRegs.ADCSOCFRC1.all = 0x00FF;
//
//keep taking samples until the results buffer is full
//
while(resultsIndex < RESULTS_BUFFER_SIZE)
{
//
//wait for first set of 8 conversions to complete
//
while(0 == AdcaRegs.ADCINTFLG.bit.ADCINT3);
//
//clear both INT flags generated by first 8 conversions
//
AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1;
AdcaRegs.ADCINTFLGCLR.bit.ADCINT3 = 1;
//
//save results for first 8 conversions
//
//note that during this time, the second 8 conversions have
//already been triggered by EOC6->ADCIN1 and will be actively
//converting while first 8 results are being saved
//
AdcaResults[resultsIndex++] = AdcaResultRegs.ADCRESULT0;
AdcaResults[resultsIndex++] = AdcaResultRegs.ADCRESULT1;
AdcaResults[resultsIndex++] = AdcaResultRegs.ADCRESULT2;
AdcaResults[resultsIndex++] = AdcaResultRegs.ADCRESULT3;
AdcaResults[resultsIndex++] = AdcaResultRegs.ADCRESULT4;
AdcaResults[resultsIndex++] = AdcaResultRegs.ADCRESULT5;
AdcaResults[resultsIndex++] = AdcaResultRegs.ADCRESULT6;
AdcaResults[resultsIndex++] = AdcaResultRegs.ADCRESULT7;
//
//wait for the second set of 8 conversions to complete
//
while(0 == AdcaRegs.ADCINTFLG.bit.ADCINT4);
//
//clear both INT flags generated by second 8 conversions
//
AdcaRegs.ADCINTFLGCLR.bit.ADCINT2 = 1;
AdcaRegs.ADCINTFLGCLR.bit.ADCINT4 = 1;
//
//save results for second 8 conversions
//
//note that during this time, the first 8 conversions have
//already been triggered by EOC14->ADCIN2 and will be actively
//converting while second 8 results are being saved
//
AdcaResults[resultsIndex++] = AdcaResultRegs.ADCRESULT8;
AdcaResults[resultsIndex++] = AdcaResultRegs.ADCRESULT9;
AdcaResults[resultsIndex++] = AdcaResultRegs.ADCRESULT10;
AdcaResults[resultsIndex++] = AdcaResultRegs.ADCRESULT11;
AdcaResults[resultsIndex++] = AdcaResultRegs.ADCRESULT12;
AdcaResults[resultsIndex++] = AdcaResultRegs.ADCRESULT13;
AdcaResults[resultsIndex++] = AdcaResultRegs.ADCRESULT14;
AdcaResults[resultsIndex++] = AdcaResultRegs.ADCRESULT15;
}
//
//disable all ADCINT flags to stop sampling
//
EALLOW;
AdcaRegs.ADCINTSEL1N2.bit.INT1E = 0;
AdcaRegs.ADCINTSEL1N2.bit.INT2E = 0;
AdcaRegs.ADCINTSEL3N4.bit.INT3E = 0;
AdcaRegs.ADCINTSEL3N4.bit.INT4E = 0;
EDIS;
//
//at this point, AdcaResults[] contains a sequence of conversions
//from the selected channel
//
//
//software breakpoint, hit run again to get updated conversions
//
asm(" ESTOP0");
}while(1);
}
//
// ConfigureADC - Write ADC configurations and power up the ADC for both
// ADC A and ADC B
//
void ConfigureADC(void)
{
EALLOW;
//
//write configurations
//
AdcaRegs.ADCCTL2.bit.PRESCALE = 6; //set ADCCLK divider to /4
AdcSetMode(ADC_ADCA, ADC_RESOLUTION_12BIT, ADC_SIGNALMODE_SINGLE);
//
//Set pulse positions to late
//
AdcaRegs.ADCCTL1.bit.INTPULSEPOS = 1;
//
//power up the ADC
//
AdcaRegs.ADCCTL1.bit.ADCPWDNZ = 1;
//
//delay for 1ms to allow ADC time to power up
//
DELAY_US(1000);
EDIS;
}
//
// SetupADCContinuous - setup the ADC to continuously convert on one channel
//
void SetupADCContinuous(Uint16 channel)
{
Uint16 acqps;
//
// Determine minimum acquisition window (in SYSCLKS) based on resolution
//
if(ADC_RESOLUTION_12BIT == AdcaRegs.ADCCTL2.bit.RESOLUTION)
{
acqps = 14; //75ns
}
else //resolution is 16-bit
{
acqps = 63; //320ns
}
EALLOW;
AdcaRegs.ADCSOC0CTL.bit.CHSEL = channel; //SOC will convert on channel
AdcaRegs.ADCSOC1CTL.bit.CHSEL = channel; //SOC will convert on channel
AdcaRegs.ADCSOC2CTL.bit.CHSEL = channel; //SOC will convert on channel
AdcaRegs.ADCSOC3CTL.bit.CHSEL = channel; //SOC will convert on channel
AdcaRegs.ADCSOC4CTL.bit.CHSEL = channel; //SOC will convert on channel
AdcaRegs.ADCSOC5CTL.bit.CHSEL = channel; //SOC will convert on channel
AdcaRegs.ADCSOC6CTL.bit.CHSEL = channel; //SOC will convert on channel
AdcaRegs.ADCSOC7CTL.bit.CHSEL = channel; //SOC will convert on channel
AdcaRegs.ADCSOC8CTL.bit.CHSEL = channel; //SOC will convert on channel
AdcaRegs.ADCSOC9CTL.bit.CHSEL = channel; //SOC will convert on channel
AdcaRegs.ADCSOC10CTL.bit.CHSEL = channel; //SOC will convert on channel
AdcaRegs.ADCSOC11CTL.bit.CHSEL = channel; //SOC will convert on channel
AdcaRegs.ADCSOC12CTL.bit.CHSEL = channel; //SOC will convert on channel
AdcaRegs.ADCSOC13CTL.bit.CHSEL = channel; //SOC will convert on channel
AdcaRegs.ADCSOC14CTL.bit.CHSEL = channel; //SOC will convert on channel
AdcaRegs.ADCSOC15CTL.bit.CHSEL = channel; //SOC will convert on channel
AdcaRegs.ADCSOC0CTL.bit.ACQPS = acqps; //sample window is acqps +
//1 SYSCLK cycles
AdcaRegs.ADCSOC1CTL.bit.ACQPS = acqps; //sample window is acqps +
//1 SYSCLK cycles
AdcaRegs.ADCSOC2CTL.bit.ACQPS = acqps; //sample window is acqps +
//1 SYSCLK cycles
AdcaRegs.ADCSOC3CTL.bit.ACQPS = acqps; //sample window is acqps +
//1 SYSCLK cycles
AdcaRegs.ADCSOC4CTL.bit.ACQPS = acqps; //sample window is acqps +
//1 SYSCLK cycles
AdcaRegs.ADCSOC5CTL.bit.ACQPS = acqps; //sample window is acqps +
//1 SYSCLK cycles
AdcaRegs.ADCSOC6CTL.bit.ACQPS = acqps; //sample window is acqps +
//1 SYSCLK cycles
AdcaRegs.ADCSOC7CTL.bit.ACQPS = acqps; //sample window is acqps +
//1 SYSCLK cycles
AdcaRegs.ADCSOC8CTL.bit.ACQPS = acqps; //sample window is acqps +
//1 SYSCLK cycles
AdcaRegs.ADCSOC9CTL.bit.ACQPS = acqps; //sample window is acqps +
//1 SYSCLK cycles
AdcaRegs.ADCSOC10CTL.bit.ACQPS = acqps; //sample window is acqps +
//1 SYSCLK cycles
AdcaRegs.ADCSOC11CTL.bit.ACQPS = acqps; //sample window is acqps +
//1 SYSCLK cycles
AdcaRegs.ADCSOC12CTL.bit.ACQPS = acqps; //sample window is acqps +
//1 SYSCLK cycles
AdcaRegs.ADCSOC13CTL.bit.ACQPS = acqps; //sample window is acqps +
//1 SYSCLK cycles
AdcaRegs.ADCSOC14CTL.bit.ACQPS = acqps; //sample window is acqps +
//1 SYSCLK cycles
AdcaRegs.ADCSOC15CTL.bit.ACQPS = acqps; //sample window is acqps +
//1 SYSCLK cycles
AdcaRegs.ADCINTSEL1N2.bit.INT1E = 0; //disable INT1 flag
AdcaRegs.ADCINTSEL1N2.bit.INT2E = 0; //disable INT2 flag
AdcaRegs.ADCINTSEL3N4.bit.INT3E = 0; //disable INT3 flag
AdcaRegs.ADCINTSEL3N4.bit.INT4E = 0; //disable INT4 flag
AdcaRegs.ADCINTSEL1N2.bit.INT1CONT = 0;
AdcaRegs.ADCINTSEL1N2.bit.INT2CONT = 0;
AdcaRegs.ADCINTSEL3N4.bit.INT3CONT = 0;
AdcaRegs.ADCINTSEL3N4.bit.INT4CONT = 0;
AdcaRegs.ADCINTSEL1N2.bit.INT1SEL = 6; //end of SOC6 will set INT1 flag
AdcaRegs.ADCINTSEL1N2.bit.INT2SEL = 14; //end of SOC14 will set INT2 flag
AdcaRegs.ADCINTSEL3N4.bit.INT3SEL = 7; //end of SOC7 will set INT3 flag
AdcaRegs.ADCINTSEL3N4.bit.INT4SEL = 15; //end of SOC15 will set INT4 flag
//
//ADCINT2 will trigger first 8 SOCs
//
AdcaRegs.ADCINTSOCSEL1.bit.SOC0 = 2;
AdcaRegs.ADCINTSOCSEL1.bit.SOC1 = 2;
AdcaRegs.ADCINTSOCSEL1.bit.SOC2 = 2;
AdcaRegs.ADCINTSOCSEL1.bit.SOC3 = 2;
AdcaRegs.ADCINTSOCSEL1.bit.SOC4 = 2;
AdcaRegs.ADCINTSOCSEL1.bit.SOC5 = 2;
AdcaRegs.ADCINTSOCSEL1.bit.SOC6 = 2;
AdcaRegs.ADCINTSOCSEL1.bit.SOC7 = 2;
//
//ADCINT1 will trigger second 8 SOCs
//
AdcaRegs.ADCINTSOCSEL2.bit.SOC8 = 1;
AdcaRegs.ADCINTSOCSEL2.bit.SOC9 = 1;
AdcaRegs.ADCINTSOCSEL2.bit.SOC10 = 1;
AdcaRegs.ADCINTSOCSEL2.bit.SOC11 = 1;
AdcaRegs.ADCINTSOCSEL2.bit.SOC12 = 1;
AdcaRegs.ADCINTSOCSEL2.bit.SOC13 = 1;
AdcaRegs.ADCINTSOCSEL2.bit.SOC14 = 1;
AdcaRegs.ADCINTSOCSEL2.bit.SOC15 = 1;
EDIS;
}
//
// End of file
//