This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377D: TMS320F28377D

Part Number: TMS320F28377D


Dear Friends,

I am using CAN in TMS320F28377D.I have referred the C2000 example files for can external transmit check.In that defualt Bit Time Calculation is given with API's.

But while finding i technical reference manual  ,I want to calculate the BRP value using the examples given 20.12.2.2 (page no- 2009) & 20.12.2.3(page no - 2010).

I didn't understand the values how he got using the equation:

{Example -1 20.12.2.2 (page no- 2009)} = (1-1)base 3 & (8-1) base 4 &(1-1)base 2 & (1-1) base6 = 0x0000700;

{Example -2 20.12.2.3(page no- 2010)} = (4-1)base 3 & (5-1) base 4 &(4-1)base 2 & (1-1) base6 = 0x00034C1;                           

Can anyone please explain me this?

Regards,

Ashrumochan.