Part Number: TMS320F28379D
Other Parts Discussed in Thread: UNIFLASH
Hello,
after succesfully flashing with the Uniflash tool, i got this error, when i pressed the "Verify Image" Button:
[ERROR] C28xx_CPU1: File Loader: Verification failed: Memory map prevented reading 0x7801C@Program
meanwhile i got out, that this is the adress of the Z1-PSWDLOCK, but i not touched this register.
Maybe thats the result, because i changed the BOOT-Pins from the default pins to other.
I added the Gel-file, maybe it can help.
Best Regards
Julian Dolderer