Part Number: TMS320F28335
Hi,
I am developing a project to perform some experiments of an algorithm implemented in a eZdsp TMS320F28335 board.
Because it is an experiment, I need to retrieve data from the DSP (values of expressions, generally) so I was thinkg of using the GUI Composer v2 to desing a proper environment to do so.
However, the on-board emulator of the Spectre eZdsp does not seem compatible with the XDS target configuration of the GUI Composer. Therefore, I have thought using the USB UART connection to do so, although the PC does not recognize the COM port when I plug in the eZdsp.
How should I proceed?
Is it for sure that I can do what I am intended with GUI Composer?
I am using Code Composer 8.2.0.
Thank you in advance.