Other Parts Discussed in Thread: DRV8301
Hi,
While working on DRV8301 kit, I checked the back emf waveform of my motor.
And it put me into a lot of confusion.
Setup: Rotated the motor externally to measure back emf.
This is the back emf waveform when measured between Line to Line (see channel 1 - yellow signal)
And this is the back emf waveform when measured from Line to Neutral. (created a neutral point by a star connected resistor network at the motor terminal - 100 ohms resistor) (see channel 1 - the yellow signal)
Why is the shape different?
My questions:
1. When we say a BLDC motor has trapezoidal or sinusoidal back emf waveform - how are they referenced. Phase to neutral or phase to phase. In my case, one looks trapezoidal in nature and other sinusoidal.
2. What impact does the shape of back emf have on the system while using FOC control?
3. The back emf waveform that you see, are they good or bad? Does the motor need improvement? How to judge?