I am trying to get a F280049C microcontroller to boot to Flash without pullups on GPIO's 24 and 32 (Zero Boot Mode) but running into an error.
I found a post trying to accomplish the same task from January here: https://e2e.ti.com/support/microcontrollers/c2000/f/171/t/655051?CCS-TMS320F280049M-TMS320F280049-How-to-set-Zero-Boot-Mode-Select-Pins-
I implemented the changes suggested to the .asm and .link.cmd files however CCS throws an error regarding the length of OTP_Boot being of length 0x1. I changed it to length 0x3 and CCS successfully built the project. I later found another post from August that made the same change to the length (http://e2e.ti.com/support/microcontrollers/c2000/f/171/t/715617).
After I checked all my changes to the .asm and .link.cmd files, I am getting an error thrown when I go into Debug mode. The code runs but only during a Debug session so it appears that the OTP isn't being set to automatically boot from Flash. I turned on verbose mode for more information and I get the following output:
...
C28xx_CPU1: Writing buffered data @ Address 0x0007801C of Length 0x00000004
C28xx_CPU1: Error during Flash programming (Flash algorithm returned error code). Operation cancelled.
C28xx_CPU1: Please make sure the memory location you are programming have not already been programmed.
...
I looked earlier in the output and it shows that CCS is writing Flash @ address 0x0007801c with length of 0x3. So is any reason why CCS is attempting to rewrite this address which is where OTP_Boot value is located? Is there some other setting(s) that aren't mentioned in the above 2 forum threads that also needs to be modified to always boot from Flash? Also is the OTP actually "one time" programmable or can it be modified again (i.e. with the above error, is it still possible to correctly write the OTP to do a Zero Boot Mode or am I going to have to replace that microcontroller?)
Thanks.