This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049: Recommended BOR threshold level for an external SVS

Part Number: TMS320F280049

Hi Experts,

 

I would like to know the appropriate BOR threshold level for an external SVS.

 

According to the datasheet www.ti.com/lit/sprs945, the VBOR-VDDIO is 2.81V(min) and 3.0V(max).

I believe that BOR occurs during the voltage range.

Furthermore, there is a VBOR-GB 0.1V(typ).

 

So, the recommended BOR threshold is 3.0V + 0.1V = 3.1V?

I would like to utilize the external SVS instead of the internal BOR function in F280049.

 

Thank you very much for your kind advice.

Best regards,

Hitoshi