Tool/software: Code Composer Studio
Hi,
I'm trying to use 28069U IC to implement a control board.
However, I don't want to use the JTAG pins to connect a computer,
I prefer to using the USB0DP & USB0DM pins to connect a computer (through USB port).
Here is a question, if I want to use(enable) USB0DP & USB0DM pins,
I have to set the USBIOEN bit in the GPACTRL2 register,
but I don't connect to computer through JTAG, how do I set the GPACTRL2 register?
Thanks in advance.
Bojun Wang