Part Number: TMDSHVMTRPFCKIT
Hello Motor control team,
Is it possible to work TMDSHVMTRPFCKIT with induction motor 380V / 220V star/triangle connection (180W 50Hz)?
(When connecting the winding of triangle).
Is it possible to connect the oscilloscope to the terminals and the DC bus while working with the motor for oscillography?
What incremental encoder can be used to work correctly with the KIT set?
Thanks.
___________
Best Regards