Part Number: TMDSCNCD28335
I am using F28335 experimenters kit for motor control and programming it through Simulink. I am using module A of EPWM to switch all the upper devices of an inverter and module B for all the lower in a complementary fashion. I need to insert dead band for rising as well as the falling edge of the PWM signals, in addition, I require complete control on module A as well as module B using continuous software force input. To insert deadband I am using Active high complementary setting in Deadband submodule of EPWM module. As soon as I use this setting I cannot individually control the A&B modules using software force, If A is kept at low the B will remain at high even if its forced to low. How can I obtain this control?